Velocity_Actual_Value
Index.Sub | 606C.0H |
Data Type | Integer32 |
Access | Read Only |
PDO Mappable | TX_PDO (1) |
Unit | User-defined velocity unit (2) |
Range |
Integer32 |
Default Value | 0 |
Store Supported | No |
Description | This object contains the current velocity of the motor. |
Notes |
(1)Available with firmware V00r74 or superior. (2)See Factor Group. |